Security


What you will find in this section:

  1. Security

Security

 

Phoenix Contact offers products and industry solutions with cyber security functions for the future-proof operation of machines, systems, and infrastructures. To protect these it is necessary to implement and continuously maintain a holistic cybersecurity concept. Security provided by the EMpro energy measurement device constitutes therefore only part of an overall concept.

Features:

  • A PIN entry protects the EMpro against improper use. Write access using the control buttons on the device and the Modbus interface is blocked if the incorrect PIN is entered.
  • The other interfaces that allow write access (REST API & BACnet) can be set to “read-only” mode.
  • All interfaces can be deactivated individually. The users are responsible for securing their networks against unauthorized access.
  • A deactivation of control buttons for configuration is possible via web server.
  • The web server of the EMpro is password protected. Write access using the web server is blocked if the incorrect password is entered.
  • A deactivation of the web server or setting the webserver to “read only mode” is possible via display.
  • Sealable connection fields prevent unauthorized opening of the screw terminal blocks.
  • Firmware uptdates optimize the performance and expand the functionality of EMpro and aim at future-proof operation.

To prevent unauthorized write access to the device, change the default PIN and password during initial commissioning of the device.

Function

Information

Web server

Display

Register

PIN change

The default PIN is 0100.

 

x

x

Password change The default password is adm1n.

x

   

 

 


EMpro online documentation
Published/reviewed: 2026-07-10, en revision 004, Version history